Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to perform a Cold Reset in logic using a SoMachine V4.3 / EcoStruxure Machine Expert Logic controller?
Issue
Is it possible to perform a Cold Reset in a logic subroutine using a SoMachine V4.3 / EcoStruxure Machine Expert Logic controller?

Product Lines
Modicon M238, M258, M241, M251, M262, HMISCU
SoMachine v4.3, EcoStruxure Machine Expert

Environment
PLC Programming software in Windows

Resolution
The two steps required are:

1. Set/write PLC_W.q_wPLCControl := PLC_W_RESET_COLD
2. Write PLC_W.uiOpenPLCControl  := 6699

For example, the Structured Text (ST) code would look like this:

IF PLCColdReset=TRUE
THEN
PLC_W.q_wPLCControl:=4;
PLC_W.q_uiOpenPLCControl:=6699;
END_IF

For more information, search for the "PLCSystem Library Guide" for the specific PLC family in the Software Help system or the User Guide PDF on our website.