Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How much current is available on the ATS48 +24V power supply?
Issue:
ATS48 +24Vdc power supply specifications.

Product Line:
ATS48

Environment:
All models and serial numbers

Cause:
None

Resolution:
The 24Vdc power supply can provide up to 200mA.