Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Alternative for standard locking system for S3X enclosures with double door
For the installation of an alternative to the standard lock from S3X enclosures with double doors by a lock with another number of key. it is necessary to replace the escutcheon by the handle reference NSYMCSX. Example of DIN barrel usable on handle reference NSYMCSX - DIN barrel made by JMP Diffusion type 1327/999 - DIN barrel made by EMKA type 1109-U1-N See instruction sheet in attachment

Schneider Electric Saudi Arabia

Attachment(s)
Alternative for standard locking system for S3X enclosures with double door.pdf [169.29 KB]