Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do any of the Altivar Drives have a Profinet option?

Article available in these languages: Spanish

Issue:
Profinet option on ATV Drives

Product Line:
ATV61, ATV71, ATV32, ATV600, ATV900

Environment:
All

Cause:
Product Selection & Services

Resolution:
Yes, ATV600, ATV900, ATV320, ATV340, ATV61, ATV71, and ATV32 offer options cards that support Profinet.
​ATV600/ATV900/ATV320/ATV340/ATV32 Profinet option card part number VW3A3627.
ATV61 / ATV71 Profinet option card part number VW3A3327.
Some older version drives may not support the Profinet option card. Be sure to verify compatibility before ordering.