How can we help you today?

Do IU_ERIO work on X80 drop

Question:
An IU_ERIO function block updates Ethernet remote I/O drop input and output modules with an optimal response time. The Ethernet remote I/O drop inputs and outputs are updated during the MAST task.
In Unity help, the illustration example is only made in terms of Quantum Ethernet remote system(140CRA31200) .
Do this function block work on X80 drop(BMXCRA321x0)

Answer:
Yes.
After the verification test, this block is working in the Quantum X80 system.
By executing the block in MAST task, the output STATUS pin is properly indicating the drop status.

Schneider Electric Saudi Arabia
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
  • Product Documentation