How can we help you today?

Does BMXEAE0300 support on X80 rack.

Question:
Modicon X80 played as the remote I/O drop of EIO system which is supported by SE Quantum & M580 platform.
The module BMX EAE 0300 is a synchronous serial interface designed for M340.
Does   BMX EAE 0300 support on X80 rack?


Answer:
Partly supported.
Currently the BMX EAE 0300 is supported on X80 of M580 platform so that user managed to select the module in Unity 8 or later version.
However, BMX EAE 0300 is not supported on Quantum X80 and user could not select the module to X80 rack in Unity.
It is set up for the marketing perspective other than technical perspective..

Schneider Electric Saudi Arabia
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
  • Product Documentation