Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to setup plus and minus speed on the ATV212?

Article available in these languages: Spanish


Issue:
Shows how to setup plus and minus speed on the ATV212.

Product Line:
ALTIVAR 212

Environment:
All serial number

Cause:
N/A

Resolution:
Follow these steps to program terminal R for plus speed, and RES for minus speed.
Frequency Mode Select (FNOD) = 5 (+/- speeds)
Logic input R (F112) = 41 (+ speed)
Logic input RES (F113) =42 (- speed)

See ATV212 Programming manual for details.
https://www.se.com/ww/en/download/document/S1A53838/