Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Part Number for the screen of an HMISTU855?
Issue:
The screen on the HMISTU855 is broken but the Processor is still working. Is it possible to replace just the screen? If so, what is the part number?

Product Line:
HMISTU,  HMIS5T, HMISTU655, HMISTU855

Resolution:
The part number for the screen module of the HMISTU855 is HMIS85W.