Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the applicable Ecodesign standards for Medium Power Transformers?
For Medium Power Transformers (voltage until 36kV, power until 40 MVA), the Ecodesign standard applicable is EN 50588. For High Power Transformers (voltage above 36kV, power above or equal 40 MVA ) the Ecodesign standard applicable is EN 50629 (still a project at the moment)