Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the cable for remote mounting the ATV61 displays?
Issue:
Trying to find the part number for the RJ45 cable to connect to the remote display, VW3A1101.

Product line:
VW3A1101

Environment:
All products of VW3A1101

Cause:
N/A

Resolution:
We offer the cables in multiple lengths

VW3A1104R10 - 1 meter
VW3A1104R20 - 3 meters
VW3A1104R50 - 5 meters
VW3A1104R100 - 10 meters