Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the risks should arcing occur between the primary voltage setting terminals and the transformer frame on energising on a TRIHAL cast resin dry type transformer?
The arcing phenomenon observed on TRIHAL cast resin dry type transformer devices is known and is not related to any equipment problem. Explanation: When a transformer is energised, the peak switching currents can reach approximately 10 times the nominal current. The time constant for 2000 KVA TRIHAL devices is approximately 0.6 sec. These switching currents generate leakage fluxes of the same duration which, as they re-close in the air, induce high currents in all the metal parts around the transformer. These induced currents trigger short duration arcing phenomena at the joints between the panels of the housing of these devices. To summarise: These phenomena are mainly seen on devices whose power is greater than 1000 KVA. They are not at all serious and are definitely not evidence of a transformer problem. Moreover, these phenomena are totally random and their intensity is dependent on the moment of energisation on the voltage sine wave.