Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the max current for the +24v internal supply on the ATV61 drive?
Issue:
Max current for the +24v internal supply on the ATV61/71 drive.

Product Line:
All ATV61/71 drives

Environment:
+24v internal power supply on ATV61/71 drive

Resolution:
Max current for the internal +24v supply is 200mA.