How can we help you today?

What is the character limitation of a power meter or gateway web page password?

Issue
If the configured password is too long, the web page authentication will fail

Product Line
EGX100

EGX300

COM'X 200

PM8ECC

PM500

ECC21

PM8000

Environment
Web server

Cause
The password fields for logging in to device web pages will accept more characters than the page's authentication permits.

Resolution
The character limitation of various devices are shown below

DevicePassword Length
EGX10012
EGX30012
COM'X 200 Over 24
PM8ECC12
PM500016
ECC218
PM80008

Schneider Electric Saudi Arabia