Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How do you reset the ATV312 drive back to its default factory settings?
Issue:
Restoring factory settings on the Altivar 312?

Product Line:
Altivar ATV312

Environment:
All ATV312 models

Cause:
Need to reset the drives settings back to the factory default to clear any user customization.

Resolution:

Note: "Scroll down" means turn the dial clockwise. "press enter" means push in on the dial.

At RDY, press enter
Scroll down to the drC menu and press enter
Scroll down to FCS ( restore config to factory settings) and press enter
Scroll down to InI and hold enter for 3 seconds unit the display flashes back to no.  Now the drive has been reset back to its original factory settings.

Review this procedure in the video provided below: