How can we help you today?

What is the QEIO X80 architecture using BMXNRP0201.

Question:
Is  BMXNRP0201 counted as a device inside QEIO X80 loop?
What is the QEIO X80 architecture using BMXNRP0201?


Answer:
The BMXNRP0201 is not considered as 1 hop in QEIO loop, its just the pure converter by physical level which does not take into account during main ring capacity calculations.

The validated QEIO X80 architecture using BMXNRP0201 is attached.

Schneider Electric Saudi Arabia

Attachment(s)
Architecture.png [69.06 KB]