Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATSU01N...LT : Where is the run command contact terminated?
Issue:
Where do I install the run command contact?

Product Line:
Altistart 01

Environment:
All models

Cause:
N/A

Resolution:
The start contact needs to provide 24Vdc to LI2.  There are multiple schematic possibilities.  See attachment for examples.

Schneider Electric Saudi Arabia

Attachment(s)
ATSU01N2 - LT W91624688 R4-2004.pdf [728.15 KB]