Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How does Vijeo Designer Runtime determine when to use Simulated SRAM?
Issue:
How does Vijeo Designer Runtime determine when to use Simulated SRAM?

Product Line:
Vijeo Designer (all versions)

Resolution:
Today in Vijeo Designer, there isn't any link between the data location settings and where the SRAM simulation file is actually stored. In fact, there is a series of checks that are done to determine the best place to store this internal file.
The algorithm is something like this:
if HMI has physical SRAM chip:
--> Start Runtime normally and use SRAM chip
If HMI has no physical SRAM chip:
check existence of Secondary Drive
--> If exists, store Simulated SRAM file on Secondary
--> else check existence of Optional.
--->If exists, store file on Optional
--->else error and refuse to start Runtime