Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is possible to upload a custom QR-code on the ATV630 Process Drive into the drive that will link the person scanning the code to a specific web site?

Issue:
Uploading custom QR-code into the drive that will link the person scanning the code to a specific web site

Product Line:
Altivar 630, process drive

Environment:
All serial numbers

Cause:
N/A

Resolution:
It's possible to manage up to 4 customized QR code. Those QR code will be fixed and accessible in one location on graphical keypad (not possible to manage on dedicated event for example).

To configure those QR code you need to use DTM (SoMove)


After this the customized QR code will be accessible in keypad menu : My preferences-QR codes