Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will the BMXP342020 or BMXNOE communicate over Ethernet/IP?
Issue:
Will the BMXP342020 or BMXNOE0110 communicate over Ethernet/IP?

Product Line:
M340, BMXNOE, BMXNOC, EIP, Modbus/TCP, MB/TCP

Resolution:
No, both P342020 and the BMXNOE support only Modbus/TCP.  To get Ethernet/IP the BMXNOC module is required.