Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the FTP user name and password for ION 7650/7550 meters?
Issue
User needs to access the FTP site for a meter.

Product
ION 7650/7550

Environment
FTP

Resolution
If Standard Security is used the defaults are:
Username: 7650
Password: [front panel password] (default is 0)

If Advanced Security is needed, it can be setup by following the below instruction:
At least 1 Security User module with "Read Access" and "Test mode Access" needs to be present and active on the meter.
Refer to ION Setup User guide on how to configure Standard and Advance Security and how to place a meter in advanced configuration.
  1. Place the meter in advanced configuration mode
  2. Open the Security User Modules folder
  3. Right click and select Insert Module to add a new module
  4. Double click the module to setup permissions and password
  5. Use the button "Password..." to configure the password
  6. Under Setup registers, ensure "Read Access" and "Test Mode Access" are set to "Yes", other permissions can be set to "No" if not needed
  7. Send the changes to the meter

How to log onto the FTP site:
  1. Enter ftp://[IP Address] in a browser or FTP client
  2. When logon is requested enter the user and password setup above,
For example, User01 will login with:
Username: user1
Password: user defined password