Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
iRIO Modbus Function Code 02, is iRIO able to read Modbus finction code 02 (input status) ?
Yes, it's possible to  configure the modbus function code 02 need  to be configured in the variable address field