Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Schneider Electric offer a soft starter with built in bypass?
Issue:
Soft starters with built in bypass.

Product Line:
ATS22

Environment:
All

Cause:
Space restrictions

Resolution:
The ATS22 softstart product line has a standard built in shorting contactor (end of start contactor).