Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why is a communications loss after changing the Com'X security settings?
Issue
Changing the Com'X security certificate causes communication loss

Product Line
Com'X 200, Com'X 210, Com'X 510

Environment
Settings >> Security >> Certificates

Cause
When the device security parameters have changed the Com'X must reestablish communications by reloading the web interface.

Resolution
Allow device to reestablish communications.

Note: If you are unable to find security certificate settings then you may need to perform a firmware upgrade.