Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does our ConneXium switches have integrated DHCP functionality?
Issue

Hirschmann mentions in new firmware for switches that they integrated DHCP server. Is this applicable for the Schneider version?

Product Line

Schneider Connexium switches

Resolution

Hirschmann firmware already supports the DHCP server functionality. However, it is not part of the features that was configured for the Schneider OEM versions.