How can we help you today?

Could not remove directory \usr\Cfg message when upgrading M241/251 firmware

  • When upgrading using Controller Assistant and USB cable, error message "Could not remove directory \usr\Cfg" is displayed.
  • When upgrading using SD card "Delete "/usr/*" (line 1) returned cleaning error" appears in SCRIPT.log file.

This is because some corrupted files can not be deleted.
To delete these files " Format "/usr" " should be added to SD card script.

In firmwares starting from v4.0.2.52 " Format "/usr" " is added automatically by Controller Assistant when generating SD cards.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre