Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Cannot change the HTTP or FTP password for the BMXNOE0110 using Web Designer.

Issue
Cannot change the HTTP or FTP password for the BMXNOE0110 using Web Designer.

Product Line
BMXNOE0110

Environment
Windows 10

Resolution
The selection for HTTP and FTP password on the target security window is greyed out and not selectable.

wery6

Due to cyber security reasons, the ability to change the HTTP and FTP passwords for BMXNOE0110 Factorycast
module using Web Designer is not allowed.   Changing of the passwords for the  BMXNOE0110 Factorycast module
must be performed from the 'Setup' web pages.