{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How do I activate/deactivate the EWF (Enhanced write filter) on Windows 7 Embedded iPC?

Article available in these languages: Czech

Issue

File writes or program installation to the main drive of a Magelis iPC are not being kept before and after a restart because the disk volume is write-protected.


Product Line

Magelis iPC, HMIG5U, HMIG5U2


Environment

Windows 7 Embedded


Cause

The main disk volume of the iPC is write-protected in order to maximize the life of the disk as well as ensuring the saved state of the disk for consistent behaviour day-to-day for applications which need it (for example a factory HMI). This is done through a feature called the Enhanced Write Filter (EWF).


Resolution

Verifying current state of EWF:

  1. Click on the** Start** button on your PC.
  2. Please now select the Run option and at the command prompt type** cmd** (make sure theres administrator rights..if not run as administrator)
  3. You will now be presented with a black command prompt window and within this will need to type – ewfmgr c:
  4. This will now return a series of results and will tell you the current state of the EWF.

The Windows Taskbar will also indicate the EWF status:

See the screenshot: "Windows Taskbar EWF State.png"

EWFMGR activate and deactivate commands to use:

To use any of the following commands then you will need to firstly navigate to the command prompt window with the following steps:

  1. Click on the Start button on your PC.
  2. Please now select the Run option and at the command prompt type cmd
  3. You will now be presented with a black command prompt window and begin typing the following commands:

ewfmgr.exe c: -Enable

Activates the EWF from the DOS cmd prompt.

ewfmgr.exe c: -Disable

Deactivates the EWF from the DOS cmd prompt.

ewfmgr.exe c: -commitanddisable

Commits changes that exist in the RAM state to the drive, then deactivates the EWF from the DOS cmd prompt

The Graphical User Interface to Activate/Deactivate EWF can also be used (EWF Windows GUI.PNG):

1. Double-click on the padlock icon and the :Enhanced Write Filter: Overview” popup should appear.

2. Select the “C:” row.

3. Click on “Configure…”

4. Select “Disable”

5. Tick the “Commit” Checkbox

6. Click OK

7. Windows Restart windows from the Start bar.

Schneider Electric Saudi Arabia

Attachment(s)

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.