How can we help you today?

Unity Pro crashed when loading a CNF file inside a TSXPBY100?

When the CNF file is loading inside the TSXPBY100, UPV10 crashed.
This is also true with Unity Pro V8.0, V8.1 and whatever the Sycon version used to build the CNF file.

A TSXPBY100 has 8 KWords of memory. Profibus slave consumes Bytes of configuration. Main parts of these Bytes are linked to the ‘Max_User_Prm_Data_Len’ parameter. The master also uses some configuration words. This crash occurs when the TSXPBY100 memory is over reached.
[((8*1024)*2)/(Slave configuration bytes)]+ master = MAX slave number

‘Max_User_Prm_Data_Len’ parameter size can be found inside the device DFB.

A Unity Pro V11.1 Hot Fix will be done for 2Q2016 in order to avoid that Unity Pro be closed. Instead of a message will pop up when this limit will be reached.