Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Device is Unauthorized When Creating a New Project in Scadapack Workbench (CAM3 & CAM5)

Problem:

After creating a new project using a SCADAPack (CAM 3) or SCADAPack E (CAM 5) template, I get the following error:
"Unable to load project c:\users\usernamexx\documents\scadapack\workbench\solutions\ScadapackProjectx\ScadapackProject\Prjlibrary.mdb with this limited license. Device is Unauthorized".

Image1

Environment:

ISaGRAF 3.55, SCADAPack Workbench (CAM3 & CAM5)

Fix:

In order to use the SCADAPack Templates in SCADApack Workbench CAM3 & CAM5 a software license is required. Please review the Licensing SCADAPack Workbench Documentation.