Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Unable to Save the Realflo Configurations

Problem:

Using Realflo v6.91.5 software, Realflo can read the configuration from the controller without any warnings but it is unable to save the file.
It comes back with the following error messages:
Unable to write to file "C:users\owner\my documents\realflo\realflo_test.tfv'
Error message 1

and:
Unable to write to file "C:users\owner\my documents\realflo\realflo_test.tfx'
Status
code=0x800004003
code meaning = invalid pointer
source=(null)
description=(null) Error message 2

Fix:

Reinstall MSXML4.DLL file.
After the driver install, un-install Realflo software. restart PC and re-install Realflo. Read the configuration from the controller and save the configuration.