Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to change the default counter interrogation time in PSE by using IEC870IP driver
Please add and change the following parameters in the citect.ini, and change the default value to what you need.

[IEC870IP]
CounterPollTimeSec       Determines how often a counter interrogation is performed.  0~32767(in second)     default value is 1800

CounterPollType             Determines the type of counter interrogation message that is sent.        0 – No freeze or reset                   default value is 1
1 – Freeze without reset
2 – Freeze with reset
3 – Reset only

You can also check the detailed information in the Driver's help.