Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the least version of Ethernet module to solve the CPU hooker issue
Background:
There used to be the hooker issue on eth module/cpu copro by which the comm. process  hooks the interaction with CPU endlessly during net broadcast storm. In this situation, the CPU is likely to go HALT due to run time overrun.

Question:
What is the least version of Ethernet module to solve the CPU hooker issue?


Answer:
Addressed by OPR20040135, the least version of Ethernet module to solve the CPU hooker issue is as indicated below---
Q-NOE  V4.3
ETY      V4.1
CoPro   V2.6