Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to re-install Connexium Network Manager without losing the authorization.
The following steps can be used to re-install the Connexium Network Manager (CNM) software without losing the authorization:
  • Start CNM.
  • Create a backup zip file by clicking on File\Save Backup.
  • Close CNM.
  • Insert the CNM installation CD
  • Run the setup for the CNM installation (This will uninstall CNM).  After the uninstall finishes, you will be prompted to run the setup again.
  • Install CNM by running the setup again.
  • Start CNM.
  • The configuration and database information should appear after starting up.  The license information should also still be preserved.
  • Restore the backup if needed.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre