Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: When to use the Internet Explorer Browser object in Vijeo Designer
Issue:
Looking for a way to view a website within the Vijeo Designer Runtime

Product Line:
Harmony / Magelis iPC or HMI targets running Windows Operating Systems

Resolution:
The Internet Explorer browser object in Vijeo Designer is only to be used with iPC or HMI targets running Windows Operating Systems. When using this object in a Windows environment, you will be able to open web pages as you would on your regular PC within the Vijeo Designer Runtime window.

When using HMIs such HMISTU, HMISTO, XBTGT, XBTGK, HMIGTO, HMIGTU, use the Multi-platform Browser Object instead. This object will allow you to open pre-downloaded files such as HTML that you include at Data Files node in Vijeo Designer.