Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the range of wavelength acceptable by ACE937 module?
Issue
Specification needed for ACE937 input

Product Line
ACE937

Environment
Sepam 20, 40, 80

Resolution
ACE937 fiber optic interface can accept a minimum wavelength of 792 nm and maximum wavelength of 865 nm. The most common wavelength, as shown in the manual, is 820 nm.