Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
MBX Driver Suite Version 8.0 is qualified to work with which Windows O.S platform ?
MBX Driver Suite Version 8.0 qualified to work with windows O.S are  32-bit and 64-bit Windows 8/7/Vista/XP SP3/Server 2012/Server 2008/Server 2003
applications, and 16-bit DOS and Windows (Win16) applications.