Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does ATV630 Process drive have PLC logic?
Issue:
Is PLC logic embedded in ATV630 Process drive?

Product Line:
Altivar 630, ATV630.

Environment:
All models, All serial numbers.

Cause:
Customer needs to use PLC logic in ATV630 drive.

Resolution:
The ATV630 Process drive does not have PLC logic built-in.