Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the default DNP3 TCP port number for scadapack E series RTU like 334E to use in scada like Vijeo Citect ?
Default TCP port number for DNP3  ​Scadapack RTU like 334E or E series can be found in E- configurator.
Go to E- Configurator menu --->  communication ---> communication settings and general tab.
As seen in figure below default number is 20000 .