Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What do the ATV61/71 1.1-1.5 status LED's indicate?

Issue:
Where can I find information on the 1.1 through 1.5 LED indicator lights?

Product Line:
ALTIVAR 61/71

Environment:
All

Cause:
Product Selection & Services

Resolution:
LED's 1.1-1.5 belong to Controller Inside Card (or similar, like a Water Solutions Pump Card).

When used with a Controller Inside Card (CIC), the LED's indicate status as shown below in an excerpt from the ATV61/71 Controller Inside manual:

ComcardLED



When used with a Water Solutions Pump Card, the LED's indicate status as shown below in an excerpt from the Water Solution Control Card User manual:
comcard




For further details see the attached files.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Attachment(s)
ATV61-71 CIC Card Status LEDs 1.1-1.5.png [101.23 KB]
ATV61_71_Controller_inside_EN_1757062_05.pdf [612.07 KB]
ATV61-71 Water Solutions Card Status LEDs 1.1-1.5.png [83.47 KB]
ATV61_Water_solution_control_card_2010_EN_1769570_05.pdf [1.18 MB]
ATV61 71 1.1-1.5 Status LEDs.pdf [203.32 KB]