Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the OFS server designed to run multiple instances based on however many users are requesting items from it?
Issue
Is the OFS server designed to run multiple instances based on however many users are requesting items from it?

Product Line
OPC Factory Server (OFS)

Environment
Windows 10 version 1902, OFS v3.62

Resolution
The OFS server is designed to run as a single instance per machine but with multiple DCOM clients.