Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to "Move" One Variable to Another in SCADAPack Workbench (ST, FBD and LD)

Some PLC programming applications have a "move" block to perform the task of assigning one variable to another. In SCADAPack Workbench (CAM3 & CAM5) ,there are multiple programming language options as it is an IEC 61131-1 environment. Each of these languages have their unique way of performing a "move" command.

In the following examples, it is assumed you have declared local variables for each POU (Program Organization Unit)

1

Function Block Diagram (FBD)

2

Structured Text (ST)

3

Ladder Diagram (LD)

4





Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: