Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the ATV 9xx Drive be placed directly within our Ethernet Remote IO main ring.?
Issue:
ATV 9xx placement directly within Ethernet Remote IO main ring.

Product Line:
ALTIVAR 930

Environment:
All

Cause:
Altivar Process ATV 9xx and M580 ERIO

Resolution:
Today, the status quo concerning ATV9xx and RIO is as follows:
- ATV9xx can be physically connected on ERIO ring and co-exists with other RIO devices on the ring,
- However, ATV9xx does not offer full RIO features i.e.: communication with it is not synchronized with PLC cycle and non-deterministic.
- It is configurable on the PLC side as DIO-type device.
Project on ATV9xx RIO features is ongoing but, we do not know the date, when ATV9xx will have full RIO features (such a date cannot be guaranteed today).