Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
On the ATV61/ATV71 Drives, why can the logic input assignments not be changed?
Issue:
ATV61/ATV71 logic input assignments modification

Product Line:
ATV61 ATV71

Environment:
All models

Cause:
Attempting to change LIx assignments in the menu 1.5 INPUTS/OUTPUTS

Resolution:
One reason may be that the drive is currently in run mode.
The logic input assignments under 1.5 INPUTS/OUTPUTS menu are read only. To change an assignment, go to the desired function and then assign that function to the logic input.