Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PM2xx meter is not available as a device type in ION Setup 3.0

Issue
PM2xx meter is not available as a device type in ION Setup 3.0

Product Line
PM2xx

Environment
ION Setup 3.0

Cause:
PM2xx meters' register map is very similar to PM7xx meters' register map and they are combined as one device type.

Resolution
PM2xx template is available as part of the "PowerLogic PM700 Series Power Meter".
General page for PM210 Type driver ION Setup 3.0

after choosing this device type, navigate to Display tab and change template options to "PM200" and click OK
PM200 ION setup