Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can my application be automatically transferred to the M580 standby PLC as soon as I transfer the application on the Primary PLC
There are two methods:
- Clear a CPU (see related topic in the manual on how to clear), set the appropriate letter (A/B), connect the HSBY link to the Primary CPU. The transfer is automatically done, but the CPU does not start because it is a cold start. Power cycle it one more time: because it is a warm start the CPU will start.
- Set the Device DDT "ECPU_HSBY_1.CMD_RUN_AFTER_TRANSFER" to 1 in the Primary CPU before plugging the paired CPU