Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
XXMIT Function Code 3 may exhibit error 11 or error 127
Goals and Symptoms

This Resolution describes the issue using the XMIT, XXMIT, or L9_XMIT Function Blocks with Function Code 3 in Unity V8, Unity V8.1, or Unity V10.


Facts and Changes

When executing function code 3 with any of the XXMIT Function Blocks, an error 11 or error 127 may be displayed and the block will not work. The issue may occur if the XMIT, XXMIT, or L9_XMIT is programmed using Unity V8, V8.1, or V10.


Causes and Fixes

The issue is resolved in:
1. Unity 8 with HotFix (UnityPro_V80_ HF0294874R) see attachments
2. Unity 11.

* A HotFix is not available for Unity V8.1 or Unity V10.
* The size of the Msg In ARRAY must be equal to the amount of words being read.
* This is a Unity solution only and does NOT require any firmware upgrades to the processors.


Additional Information

Schneider Electric Saudi Arabia

Attachment(s)
UnityPro_V80_HF0294874R.7z [4.88 MB]