Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you clear the fault history in an ATV61 or ATV71 drive?
Issue:
Clearing the fault history in an ATV61 or ATV71 drive.

Product line:
ATV61, Altivar 61, ATV71. Altivar 71

Environment:
All

Cause:
Customer has a new installation, and it faulted on Main overvoltage.  They corrected the problem, and want to clear the history for the end user.

Resolution:
No, it is not possible to clear or reset the fault history on the drive.