Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I check the logic inputs are working on an ATV312 drive?
Issue:
Customer is not sure if the inputs are working.  Drive is not running.

Product line:
Altivar 312, ATV312

Environment:
all

Cause:
n/a

Resolution:
Go under the SUP menu to LIA-.  Under LIA-, select parameter LIS (not LI5A).  This will show the Logic inputs from LI1 to LI6.  The dash mark will be high (closed) or Low (open).  See the attached page from the programming manual, BBV46385 as reference.

Schneider Electric Saudi Arabia

Attachment(s)
BBV46385_03 ATV312 IO Map.pdf [21.5 KB]