Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to setup a reverse command on ATV61/71 using I/O profile mode.

Article available in these languages: Spanish

Issue:
Command to run reverse via Communication

Product Line:
ATV61 ATV71

Environment:
All models using with communication card in I/O profile

Cause:
None

Resolution:
In I/O profile parameter rrS [Run Reverse] can be assigned to any bit between 1 and 15 according to the following protocol:
With integrated Modbus in [I/O profile]   [C101] to [C115]:
With integrated CANopen in [I/O profile] [C201] to [C215]:
With a communication card in [I/O profile] [C301] to [C315]:
With a Controller Inside card in [I/O profile] [C401] to [C415]:

Example: If you want to run reverse over the Ethernet IP network you will need to go to menu 1.5 [INPUTS / OUTPUTS CFG] and assign "rrS" to C302.