Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Sag/Swell module configuration / Hysteresis / ChangeCrit setup - HowTo Excel Workbook
Sag/Swell module configuration / Hysteresis / ChangeCrit setup

Product Line:
ION7550 / ION7650 / ION8650 / ION8800 / PM8000

Resolution:
Use the attached excel workbook in order to configure the Sag/Swell module.
See how the module behaves under different setup scenarios.

Schneider Electric Saudi Arabia

Attachment(s)
Sag-Swell-setup-HowTo.xlsx [140.98 KB]